Cancel
Showing results for 
Search instead for 
Did you mean: 

wrap curve

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I try wrap curve.

 grap.jpg

 

It should be projected onto the hemispherical shape that is not cylindrical.

 hemispherical.jpg

 

What way?

12 REPLIES

Re: wrap curve

Phenom
Phenom

You can not use this command with not developable surfaces.

 

Re: wrap curve

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator
OK.
Is there another way function?

Re: wrap curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry i have no solution to this ..using wrap curve but will it be possible for you to use PROJECT CURVE instead (with equal arc length)

pr_wr.jpg

Re: wrap curve

Experimenter
Experimenter
Sorry..
project does not fit.

Re: wrap curve

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

You can send your file to my email : nguyennhotu.hocthoinhe@gmail.com

Re: wrap curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try wrapping the curves to a similarly sized cylinder then project the wrapped curves onto the hemispherical surface (use the "along face normal" direction option). It may require significant tweaking of the input curves to get what you want.

 

If you have access to NX 11, you may be able to make use of the new "flatten surface" command. Supposedly it allows you to flatten a surface, create curves on it, and map the curves back onto the surface.

Re: wrap curve

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

In this simple case, Global Shaping should be able to provide a solution (if you have the license).

 

Regards, Ben

Re: wrap curve

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator
I have access to NX11.
but I not found to "flatten surface"

Re: wrap curve

Legend
Legend

For the simple example you show it can be done analytically (program/journal) since on a sphere or torus section the lines for the simple planar lines would produce arcs in the latitude and longitude direction on the sphere or torus.

 

Frank Swinkels