Cancel
Showing results for 
Search instead for 
Did you mean: 

zombie dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have a drawing of a small assembly; "replace component" was used on one of the parts. The drawing was then updated and most of the dimensions updated or went into the "retained" state as expected. However, a few dimenions went into a zombie-like state; they do not update with the model, but they are not "retained" either. In fact, they cannot be selected for editing or deletion. Has anyone seen this before? NX 9.0.3.4

3 REPLIES 3

Re: zombie dimensions

Gears Phenom Gears Phenom
Gears Phenom

Are these dimensions on a only visible layer?

 

Ciao

 

C.

Re: zombie dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe that the layers were set to visible and selectable. Unfortunately, I cannot check now because it was a coworker's file and I think that he has deleted the sheet and started it over. Thanks for the suggestion, if this happens again I will definitely double check the layer settings.

Re: zombie dimensions

Siemens Legend Siemens Legend
Siemens Legend

The function i think is the best at selecting "odd balls" is the good old Information-Object.

  ( yes, that function that the Ribbon UI designer doesn't think anybody is using...)

When this are non-selectable for different reasons, Info-Object normally selects.

 

Regards,

 Tomas