Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Printing NX 11 STL Export Settings

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

3D printing is booming–big time. And since most 3D printers accept STL exports, engineers are using the export format more and more.

I’ve experimented with 3D printing using different settings of the STL export format. In this article, I’ll share my experiences with you. For the sake of accuracy, for these tests I used NX 11 and an Ultimaker 3D printer.

 

My first experience with round 3D parts

The first time that I printed a round 3D part, I noticed that the shape had segments along the outer edge. Contrary to my expectations, the segments were linear, like an optimized circle.

I opened the slicer tool Cura to check if I could see the segments in my part. Cura did not show any segments, so this was not caused by my part. Also, I had successfully printed 3D parts with round edges in the past, so the culprit seemed to be the settings of the STL export.

Test

I created 3 test discs, each with a diameter of 70mm. I exported them with different STL settings. To easily identify each disc, I added the name of the settings and values as text on the top surface.

 

Settings

Chordal Tolerance

(mm)

Angular tolerance
(deg)
Default settings
The first disc was exported with
the default settings of NX11.
  0.08   18
Lowest settings
The second disk contains the
lowest possible settings of NX.
  0.0025   1
Middle settings
The third disc was exported with
the values between the default and
lowest settings.
  0.04125   9

 

As you can see in the photos below, in the default settings, the segments are visible. The disc with the lowest settings gives the best results: you can hardly see or feel the segments. The last disc still has some segments visible, but way less than the default settings.

 

 

Default top_small.jpgDefault settingsLowest top_small.jpgLowest settingsMiddle top_small.jpgMiddle settings

 

Default_detail.jpgDefault settings side viewLowest detail.jpgLowest settings side viewMiddle Detail.jpgMiddle settings side view

 

Tips

  1. Before you do an STL export from NX 11, you can turn on the option “Triangle Display”. This option will show the angle faceting of your STL export.
  2. If you want the best results out of your 3D prints, you should experiment with the NX 11 settings. To change your settings:
    • For each export, change the default settings
    • To change the default settings for all STL exports, go to “setting gateway -> translators -> STL export”.

NX_export_tip.jpg

 

Summary

When you find that you have segments instead of round edges in your printed 3D parts, please check the settings of the STL export.

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions
Comments
Phenom
Phenom

Thanks for this tip. I struggled to get the Customer Defaults set as you show in your example. I found that I can set a default angle of 1 deg in customer defaults, and it accepts it, but this value is not used in the STL Export as the default. I found that if I set the value to 2 deg, it does accept it. Maybe a value of 1 deg works, but it won't let me set the default value to that as a customer default.