Cancel
Showing results for 
Search instead for 
Did you mean: 

Boolean, Blend, and Draft Enhancements

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

blend_draft_boolean.pngFeatures with greater robustness & performance significantly simplify the process of creating and editing complex shapes.

 

New capabilities include:

 

  • Improvements in the robustness of creating and editing variable radius edge blends
  • Improvements in the robustness of creating and editing tangent matched body drafts
  • Up to 40% improvement in the performance of Booleaning large patterns of rib geometry
Tod W. Parrella
Contributors