Cancel
Showing results for 
Search instead for 
Did you mean: 

Boolean Error Display in NX 11.0.1

Siemens Creator Siemens Creator
Siemens Creator

The core Boolean features – unite, subtract, and intersect – are enhanced in NX 11.0.1 to better communicate non-intersecting bodies with error display.

 

The enhancements are summarized in the bullets below. The term “culprit” refers to an object that causes as error.

  • If a body is a culprit, error display will be applied to the body itself rather than to the edges of the body. Likewise if a face is a culprit, error display will be applied to the face rather than to the edges of the face.
  • Error display is applied to the culprit body, target OR tool, rather than both target and tool.
  • For multiple tools where a subset is a culprit, error display is applied to the culprit tools only, rather than all tools.

 

In the following example, you will see tool bodies subtracted from a target body. The gray body is the target.

  • The green tool completely intersects the target.
  • The yellow tool does not intersect the target; it is vertex-coincident with the target.
  • The blue tool does not intersect the target; it is edge-coincident with the target.
  • The pink tool does not intersect the target.Boolean1.jpgMultiple tools

Please excuse the academic examples. They are simple in order to illustrate the concept and not a reflection of my limited ability to model objects. 

 

As you select tool bodies, the culprits – yellow, blue, and pink – will report errors indicating they do not intersect the target. As illustrated below, the culprits are displayed with the error color. The green tool does intersect the target and a preview of subtract is applied.Boolean2.jpgCulprit display with error color

 

Notice that the target body is not displayed with the secondary select color. The single target body is obvious. Secondary display obscured the preview and, in combination with error display, produced more clutter than clarity.

 

In the following example, the blue tool intersects the gray target. The cylinder is tangent to the top face of the block; thus, it is coincident. Unite will succeed. Subtract will not. Subtract would produce infinitely thin volume where the cylinder is tangent to the face of the block. Error display is applied to the faces of the cylinder and the block as visual indication of where the coincident condition exists.Boolean3.jpgTangent coincidence

 

 

 

 

 

Eric
Contributors