Cancel
Showing results for 
Search instead for 
Did you mean: 

Edge Blend Variable Radius Point Along a Chain in NX 11.0.1

Siemens Creator Siemens Creator
Siemens Creator

Edge Blend is enhanced in NX 11.0.1 to define variable radius points relative to a chain of edges.

Prior to this enhancement, an arc length location of a variable radius point was relative to an individual edge. The example below is a preview of an NX 11 edge blend feature with variable radius points. The location of the variable radius point is 50% arc length.

KB2.jpg50% arc length

 The location of another variable radius point is also 50% arc length, because the arc length is measured along and relative to an individual edge.

KB1.jpg50% arc length

In NX 11.0.1, an arc length location of a variable radius point is relative to a chain of edges. In the example below, the location of the variable radius point is 26% arc length along the chain of edges selected.KB4.jpg26% arc length

The location of another variable radius point is 82% arc length along the chain.

KB3.jpg82% arc lengthWhen the geometry of the model changes, the blend will update. The variable radius points change physical location to maintain their relative location along the chain of edges.

KB6.jpg
KB8.jpg

 

The physical length of the chain has changed considerably, and the location of the 26% variable radius point remains at 26% arc length along the chain, but the physical location has changed.

KB9.jpg26% arc length

I can easily change the location of the point along the chain to influence the shape of the blend. I can drag the point along the chain or key in an arc length value.KB10.jpgChange location to 34% arc length

Eric
Contributors