Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit Mold Base Components in NX 10

Community Manager Community Manager
Community Manager

In today's tutorial, you will learn how to configure an interchangeable mold base in NX 10. Thank you @Jahnsen for this article, which originated as a reply to a question on the NX Design Forum

 

To edit the parameters of each component in the Mold Base Library, select the dropdown button beside the component. The selected component will be highlighted (as seen below) and will show the component's detailed information.

mold edit.JPG

To add or edit mold base plates, or to change the mold type, simply edit the parameters. All parameters are listed in the details of the Mold Base Library. 

 

mold type.JPG

 


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Contributors