Cancel
Showing results for 
Search instead for 
Did you mean: 

Move Linked Objects NX 11.0.1

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Previously, you could only move non-associative features using Move Object. Associative geometry is linked so that if one is modified, the other will change when the assembly or part is updated. 

NX 11.0.1 adds an associative Move Object feature to allow linked objects to be moved when position dependencies have been previously used to locate the object.

When attempting to move the highlighted object shown below the Alerts directs you to check the Asociative selection.

 

Move Object AlertMove Object Alert

Once the Associative option is active, the object can be moved positioned via Move Object.

 

Associative OptionAssociative OptionExamination of the PNT shows the addition of the Move Object feature.

 

Move Object FeatureMove Object Feature

 

 

 

 

 

 

 

Contributors