Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 Variable Offset Face

Community Manager Community Manager
Community Manager

NX 11 introduces the new Variable Offset Face functionality, which makes it easy to create complex offsets in geometry very quickly. The steps in this tutorial will walk you through the process of using the command.

 

NX 11 variable offset face 1.jpg

 

In the example shown today, we begin with geometry that contains four intersecting planes. Open the Variable Offset Face command and select the primary target face to start. Next, select each individual face where you want to create the offsets.

 

NX 11 variable offset face 2.jpg

  

Notice that as we highlight each particular face, we see two vectors appear on either side of the geometry. We can grab on to the vector and drag the face. In this case, our projection direction (located in the dialog underneath Region Boundary) is set to Normal to Face. We can drag the offset in two directions.

 

NX 11 Variable offset face.gif

  

Sometimes it may be necessary to create a more gradual transition between surfaces than an offset can provide. Notice there is also the option to create a bridge. The Bridge Continuity setting in the Variable Offset Face dialog contains two options: Connected and Tangent. Create either a straight bridge (connected) or a more gradual slope between surfaces (tangent) using these options.

 

NX 11 variable offset face 3.jpg

  

Select complete, hide the additional geometry, and the Variable Offset Face is finished. Watch the NX Quick Tips video with Sam Kuan to see these steps in action and follow along if you have NX 11.

 

(view in My Videos)


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Contributors