Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.1 MBSE and NX 12.0.2 MBSE

Siemens Phenom Siemens Phenom
Siemens Phenom

 A number of enhancements have been added to the NX MBSE process related to the Key Performance Interface (KPI) Validation gadget to improve workflows.

For load efficiency components need only be particularly loaded for requirement status to be viewed in the KPI report. To see the full information, such as check formula, MB3 Open Component Fully is now available.

NX 12.0.1 - SDPD Open Comp.png

 

In the KPI gadget the MB3 options familiar to you in the Requirements Validation report are now available so that adhoc requirements can be added in the report.

NX 12.0.1 - SDPD MB3req.pngNX 12.0.1 - SDPD MB3check.png

 

Also columns in the report for Source and Source Details have been added.

 

NX 12.0.2 MBSE 

 

Within the Systems Engineering process in Active Workspace it is now possible to create Measurable Attributes for point coordinates with a deviation limit. These can be associated to NX via an Analysis Request and displayed in the KPI gadget the same as adhoc point requirement checks.

Steve V