Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12: Tooling (MW and PDW) - Material attribute enhancements

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Users will be able to see the difference in the component attribute whether the assigned material for a part is the one provided by the NX standard material library or one configured specific to tooling applications

 

Here is an example of materials defined in tooling applications same as the one provided by NX standard materials library

BOM_3.pngBom_Data.xlsx

If the user assigns the materials in tooling applications which exist in NX standard material library, the component attrbute will be as shown below
BOM_1.pngNX 12 Component Attribute

If the user assigns the materials in tooling applications which is specific to the one defined in tooling applications, the component attribute will be as shown below

BOM_2.pngNX 12 Component Attribute

 

Contributors