Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Quick Tips - NX 9 Fit Surfaces

Community Manager Community Manager
Community Manager

You can fit surfaces to facet bodies, curve features or groups (point sets or point groups) as part of a reverse engineering workflow with the NX Fit Surfaces command in NX 9. 

 

Tod Parella shows you how to take advantage of the Fit Surfaces command in NX in this NX Quick Tips video. 

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

 

You can fit five types of surfaces.

 

Freeform

You can control the degree and number of patches, patch uniformity and fit direction. You can also control the boundary definition and smoothness of the fitted surface.

 NX Fit Surfaces 1.jpg

Plane

You can specify a direction constraint for a planar surface so that the plane normal is parallel to the specified direction.

 

Sphere

You can specify a radius value constraint for a spherical surface.

You can create an open or closed spherical surface.

 NX Fit Surfaces 3.jpgNX Fit Surfaces 4.jpg

Cylinder

You can specify a radius value constraint for the cylindrical surface. If you apply a direction constraint, it is applied to the center line of the cylinder.

You can create an open or closed cylindrical surface.

 NX Fit Surfaces 2.pngNX Fit Surfaces 3.png

Cone

You can specify an angular constraint for a conical surface. When you have an angular constraint, the half angle is fixed to the value you specify.

If you apply a direction constraint, it is applied to the center line of the cone.

You can create an open or closed conical surface.

For more details, check the NX 9 Help documentation.

NX Fit Surfaces 4.pngNX Fit Surfaces 5.png

This post originated in the NX Design Blog. You can view original comments on this post here.

Contributors