Showing results for 
Search instead for 
Do you mean 

NX Quick Tips – NX 9 Rib Construction

by Siemens Phenom Siemens Phenom ‎02-04-2015 04:14 PM - edited ‎02-06-2015 02:07 PM (1,055 Views)

You can use Rib Command in NX to add a thin-wall rib or rib network to a solid body by extruding an intersecting planar section.

 

Ribs are created based on a planar section of curves. The section can be any combination of curves.

 

  1. A single open curve with no other curves’ endpoint connected
  2. A single closed curve or spline
  3. Connected curves may be open or closed
  4. Y-junctions

 

In this NX Quick Tips video, I show you some new rib construction techniques in NX 9.

 

 

This post originated in the NX Design Blog. You can view original comments on this post here.

Contributors