Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Shortcut Keys - View Full List and Create Custom Keys

Community Manager Community Manager
Community Manager

Shortcut keys help you to eliminate mouse clicks and work more efficiently. You might only need to memorize a few for those tasks and commands you perform most regularly, but trust me, it will be well worth the minor effort up front once you're sailing through your work. Anything to make life a little easier, right?

 

You can pull up the full list of available shortcut keys in NX at anytime (I'll show you how in this tutorial!) but it's helpful to have a reference sheet handy until you get around to memorizing them. Feel free to bookmark this article, or you can even download a printable copy of the list included as an attachment.

 

You can also create custom shortcut keys in NX in addition to the standard OOTB ones listed here. Customization in NX helps to improve your workflow and maximize efficiency. Custom keys are great for particular specialized tasks you find yourself performing daily that maybe aren't commonly used by others.

 

Let's start with how to find the full list of standard keys in NX. There are a few ways to do so:

  • Type Shortcut Keys in the command finder
  • Go to Menu>Information>Custom Menu> Shortcut Keys

These include the standard copy, paste, new file commands that we are all used to, along with some CAD specific shortcuts such as extrude, sketch, etc.

 NX Shortcut Keys.jpg

 

Now, let’s look at how to create your own custom commands.

 

First, you will need to open the Customize window:

  • Ctrl+1 opens Customize directly
  • Go to File>Customize

Once in Customize, you will want to select Keyboard. This opens a new window called Customize Keyboard where you can both see existing keyboard shortcuts or you can enter your own to create new ones. Simply type and hit enter to add.

 custom shortcut keys 2.jpg

Hopefully this article helped you! Be sure to share it with your peers, particularly with anyone who is new to NX.


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Comments
Pioneer
Pioneer

F4 to repeat command

Experimenter
Experimenter

Can we assign  "make current feature" to any of the keys??

Siemens Legend Siemens Legend
Siemens Legend

Yes you can assign a key for "make current feature"

 

Regards

 

Paul

Experimenter
Experimenter

I am trying to find a way to create a hotkey for "Reverse" also known as "reverse last constraint".

 

When i open the customize window (<ctrl>+1) and i type in the search bar for "reverse" the only command that comes up is "reverse normal"

 

so with the customize bar open, i click on a constraint in my constraint navigator and it confirms that the command is called "reverse".

 

I have tried searching through the categories in the "customize keyboard" window but i can't seem to find the "reverse" or "reverse last constraint" command to setup a hotkey.

 

Can someone please tell me where IN THE CUSTOMIZE KEYBOARD window (since there is no search function in here apparently...) to find the "reverse" or "reverse last constraint" command is?

 

thanks so much!

 

Screenshot (119).png

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Unfortunately the Reverse Last Constraint 'command' you refer to is an option on a dialog. It is not a command on the menubar/ribbon. This means a user cannot add a shortcut to it.

You could file an ER for this, I think it is a good idea to do this.

 

Regards, **bleep**

Experimenter
Experimenter

Apologies, i don't know how to file an ER. Link me and I'd be happy to?

 

thanks

Contributors