Cancel
Showing results for 
Search instead for 
Did you mean: 

Precise Structure column in NX Assembly Navigator is synch'd with the TC Structure Manager.

Siemens Theorist Siemens Theorist
Siemens Theorist

In NX 12 the Precise Structure column in the Assembly NaviPrecise Structure Column.JPGgator is synch'd with the Precise column in TC Structure Manager.

  • The Assembly Navigator now displays an icon to indicate “Precise” for each assembly loaded precise or a part with an immediate parent assembly that is loaded precise.
  • To set an assembly as Precise in Teamcenter, RMB on an assembly in the Assembly Navigator and select “Set Precise on Save”.
  • The “Precise Structure” column for these assemblies initially indicates “Modified” until saved.
  • “Save Precise Assembly” command is removed.

Customer Value

  • Column values are consistent with Teamcenter Structure Manager.
  • Set a product structure node to precise inside NX

 

(view in My Videos)

Comments
Siemens Visionary Siemens Visionary
Siemens Visionary

Hi Stewart,

 

   Thanks for the information. My customer does not want to work in the Precise assembly. And would like to be able to hide that functionality from the user in NX12. This could be done in NX10 customer defaults as shown below. How can the customer get this functionality in NX12?

 

Mark

 

NX10 customer defaults.png

Siemens Theorist Siemens Theorist
Siemens Theorist

Hi,

Apparently the NX 10 customer default above would not hide the Save As Precise command, but instead it would disable saving an imprecise assembly as prescise even if the command was executed.  A Customer Defualt that would hide the NX 12 command is an Enhancement Request (ER9282344) that is currently under consideration.

Stew

Contributors