Cancel
Showing results for 
Search instead for 
Did you mean: 

Retained Chain/Baseline Dimensions in NX 11.0.1

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

A change introduced in NX 11.0.1 makes it easier to determine which dimension(s) in a chain or baseline dimension set need to be repaired.

When a dimension is marked as retained in a chain or baseline dimension set, the entire set is also marked as retained. Now the dimension status will indicate which dimension is the cause of this change, so you can easily determine which dimension(s) to repair in the set. 

 

NOTE: Status messages in NX are shown as tooltips for objects on pre-selection and shown in the status line on pre-selection and selection.

chain_helathy.pngHealthy chain dimension set.chain_retained.pngStatus on retained dimension in chain dimension set.