Cancel
Showing results for 
Search instead for 
Did you mean: 

Self-intersecting Surface Alerts in NX 11.0.1

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

When performing a series of surface commands in NX 11.0.1, you will be warned if the output faces intersect themselves.

 

An alert will appear in that case:

 

a.png

You can ignore the warning and proceed. In that case, the feature will be marked up in part navigator with a warning:

b.png

 

This applies only to self-intersecting faces, not two different faces of the same feature that intersect.

 

Enhanced Commands

The self-intersection alert has been implemented for following surface commands:

  • Law Extension
  • Section Surface
  • Studio Surface
  • Through Curve Mesh
  • Through Curves
  • Ruled
  • Bridge
  • Swept
  • Styled Sweep
  • Variational Sweep
  • Sweep Along Guide
  • Tube
  • Silhouette Flange
  • Styled Blend
Contributors