Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet Metal: Flange Enhancements #2

Siemens Phenom Siemens Phenom
Siemens Phenom

Following on from the success of the NX12 we now have even more enhancements in NX12.0.2.

The flange command has been further enhanced to include a new length measurement method and an additional placement option.

 

The flange length can be defined by a tangent measurement method that’s consistent with the DIN6935 standard measuring the feature of an obtuse (internal) angle from the outside intersection point and from the face tangent for acute angles, typical for Vernier calliper measurement methods.

flangetangent1.pngOutside intersection measurementflangetangent2.pngFace tangent measurement

 

 

 

The inset options have been revised to include an additional ‘Material Inside’ option for greater control of position.

flangeInset1.pngInset Options