Cancel
Showing results for 
Search instead for 
Did you mean: 

Tooling: Electrode Improvements

Community Manager Community Manager
Community Manager

New to the latest release of NX for mold tool & die features electrode improvements. With the new electrode improvements you have full coverage of the electrode design workflow while eliminating many manual modeling methods. 

 

Electrode Enhance.png

 

What's new? 

Copy electrode

  • Users can transform the electrode blank using Csys (CSYS to CSYS) in the copy process in addition to face to face method
  • Users can select a face or planes or existing planes as mirror plan during the process

Only top part

  • Introduced options to create the electrode assembly only based on the top part
  • As needed, user can add the blank or other operations based on this

Slope_blank

  • New option to design blanks at an angle
  • EW_HOLDER_CYSY and EW_HOLDER_ROUTE_CSYS are used to calculate the sparking positions and to output the machine coordinates start and end location
#IngenuityisNX