Cancel
Showing results for 
Search instead for 
Did you mean: 

Weld Assistant – New Marker Symbols

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Support for additional marker types allows more configuration choices and allows more distinction between discrete joint types. The Weld Assistant allows each customer the ability to configure the symbols that will be used to designate a specific joint type. For example a spot weld joining 2 components may have a different symbol then one that connects 3 or 4. With this release the choice of available markers has now been expanded.

new marker symbols.png

  • Added 30 additional Markers that can be assigned to discrete joint types
  • Markers appear as a representation of the assigned joint type
  • Supports multiple panel symbol progression strategy
  • Very high quality renderings