Cancel
Showing results for 
Search instead for 
Did you mean: 

Applying PMI Cylindrical Dimensions using intersection curve

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hi All, 

I tried to create a PMI Cylinderical Dimension using intersection curve (Refer Attached Image). During creation of PMI, I am selecting the user defined plane XZ and select the intersection curves start point. But the diameter value has shown in the PMI is upside down / mirrored position. 

Kindly do the needful to fix this issue.

 

PMICylindericalDimension.png

8 REPLIES
Highlighted

Re: Applying PMI Cylindrical Dimensions using intersection curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Manikandan_R,

I have checked this in NX 11 (11.0.2.7). It works fine for me.pmi_CYL.JPG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Applying PMI Cylindrical Dimensions using intersection curve

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

1. Orientation->Select 'User Defined Plane'

2. select XZ-Plane and create the dimension

 

Check the dimension orientation now.

Re: Applying PMI Cylindrical Dimensions using intersection curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

What if you choose XZ plane in the top options itself?

312.jpg

 

Is there any specific reason you are using the User Defined csys?

 

Looks like the csys directions you choose are directed in other directions.

322.jpg

 

Best Regards

Kapil

 

 

 

 

Re: Applying PMI Cylindrical Dimensions using intersection curve

Siemens Phenom Siemens Phenom
Siemens Phenom

@Manikandan_R wrote:

1. Orientation->Select 'User Defined Plane'

2. select XZ-Plane and create the dimension

 

Check the dimension orientation now.


Works!pmi_CYL_1.JPG

 

Can you share that particular part file?

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Applying PMI Cylindrical Dimensions using intersection curve

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Another option is to add a PMI Section View, then create your Cylindrical dimension in the view.  This is my preferred method because you often have multiple cylindrical dimensions, not just one.  Also, the PMI Section Views automatically transfer to the JT file, so you can view them in Vis.
Sectionview.png

Rick Hebert
NX Magician
Used NX (Unigraphics) since 1984
Houston, TX, USA

Re: Applying PMI Cylindrical Dimensions using intersection curve

Siemens Phenom Siemens Phenom
Siemens Phenom
One note of caution about applying PMI to curves in a PMI section view:

In some cases, the PMI section curves can not be reused by downstream applications. If you intend to reuse the PMI in your model, it is recommended that you create associative model curves instead of using the PMI section curves. And then attach your PMI to the associated model curves. Make sure to include these associated curves in your Model reference set, or other valid reference set, when exporting the PMI in a JT file.

Re: Applying PMI Cylindrical Dimensions using intersection curve

Pioneer
Pioneer
U will get same result of u select x-z plane for the above example. Actually by selecting plane we are choosing the plane in which dimension will be placed . U can select any plane as per your requirement.

Re: Applying PMI Cylindrical Dimensions using intersection curve

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Yes. That's correct. The Csys orientation is incorrect as it's shown in the image above.

It's about which axis that we are setting as horizontal & vertical. So I am setting the horizontal & vertical axis explicitly. Now it's working fine as intent.

 

PMICylindericalDimensionCsys.png

Applying PMI Cylindrical Dimensions using intersection curve

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hi All, 

I tried to create a PMI Cylinderical Dimension using intersection curve (Refer Attached Image). During creation of PMI, I am selecting the user defined plane XZ and select the intersection curves start point. But the diameter value has shown in the PMI is upside down / mirrored position. 

Kindly do the needful to fix this issue.

 

PMICylindericalDimension.png

NX PMI MBD
NX PMI MBD

This group is dedicated to the topics of PMI (product and manufacturing information) and MBD (model-based definition) in NX.

If you have a question, please post it in the NX Design Forum.

We also recommend you be a PLM World member, as this group supplements an annual roundtable at PLM Connection.

Members (257)