Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

PMI Parallel to Screen Display

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

In NX 11.0.1 the NX PMI application was enhanced to support the display of PMI on a single annotation plane that does not rotate with the model. This enhancement provides improved interpretation and supports standards-compliant display for general notes and special notations placed on a model. Setting a PMI display instance to display Parallel to Screen Display is easy and can be done by accessing the setting via the MB3 menu or PMI Preference.

 

parallel.png

 

 

An optional Lock Size and Position setting is also available to maintain the size and position of the PMI during pan and zoom operations. Support for leaders is planned for NX 12. I look forward to any feedback you have on these enhancements or suggestions you might have to further enhance NX PMI.

Regards,

Dave Wingrave

NX Product Manager, Model Based Definition

1 REPLY

Re: PMI Parallel to Screen Display

Theorist
Theorist

 Hi Dave,

Thanks for this option. This option really helps in placing general annotations. Now, i want to place an annotation at a corner in a model view such a way that the notes doesn't interfere with geometry. May be at first instance i can place it manually but later if geometry changes, how can i make sure that it won't get intefere with geometry?  do i need to change the location of annotation manually?

 

Thanks and regards
Pardha

Highlighted

PMI Parallel to Screen Display

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

In NX 11.0.1 the NX PMI application was enhanced to support the display of PMI on a single annotation plane that does not rotate with the model. This enhancement provides improved interpretation and supports standards-compliant display for general notes and special notations placed on a model. Setting a PMI display instance to display Parallel to Screen Display is easy and can be done by accessing the setting via the MB3 menu or PMI Preference.

 

parallel.png

 

 

An optional Lock Size and Position setting is also available to maintain the size and position of the PMI during pan and zoom operations. Support for leaders is planned for NX 12. I look forward to any feedback you have on these enhancements or suggestions you might have to further enhance NX PMI.

Regards,

Dave Wingrave

NX Product Manager, Model Based Definition

NX PMI MBD
NX PMI MBD

This group is dedicated to the topics of PMI (product and manufacturing information) and MBD (model-based definition) in NX.

If you have a question, please post it in the NX Design Forum.

We also recommend you be a PLM World member, as this group supplements an annual roundtable at PLM Connection.

Members (239)