Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

PMI in reusable object

Valued Contributor
Valued Contributor

Hello, 

 

I would like to define an reusable object with my PMI's is that possible? 

Is there any other way to save an feature with PMI's so i can reuse it? 

 

Thank you

NX 11.0.1.11
7 REPLIES

Re: PMI in reusable object

Siemens Phenom Siemens Phenom
Siemens Phenom

In context of Native NX, you can define a part with PMI's and add it to the reuse library source folder.

 

1.PNG

 

When you want to reuse such part, It will get added as a component into the assembly. But PMI of component will not be visible. You need to use WAVE PMI Linker command to view those PMI at root assembly level.

 

2.PNG

 

When you select the required PMI, those will get added to Part navigator along with associative linked body.

 

3.PNG

 

However if you do not want part (with PMI) to get added as component in ASN, you can simply open/load the required part and use WAVE PMI Linker command so that PMI and associative linked body gets created only.

 

4.PNG

 

Hope, This will help! Smiley Happy 

 

Re: PMI in reusable object

Valued Contributor
Valued Contributor

Hello, 

 

thank you very much Smiley Very Happy

 I have my PMI in a "lightweight section" model view, 

but the only model view i can select is the isometric.

I would like to use my intersected view is that possible. 

 

 

NX 11.0.1.11

Re: PMI in reusable object

Siemens Phenom Siemens Phenom
Siemens Phenom

You mean, Model View dropdown (Within Wave PMI Linker)  shows 'Isometric' view only, Is it?

Re: PMI in reusable object

Valued Contributor
Valued Contributor

yes exactly what i meant

 

NX 11.0.1.11

Re: PMI in reusable object

Siemens Phenom Siemens Phenom
Siemens Phenom

I have created a lightweight section view and a section view with PMI. Also added PMI in Right, Trimetric View. One thing I observed is, In WAVE PMI Linker under Model Views only those views are visible in which PMI is created. It Lists views (Standard,Section) except Lightweight Section View. I tried this using NX 10. Need to check this in NX11, unfortuantely I can't. Smiley Sad

 

5_1.PNG

 

 6_1.PNG

 

 

Re: PMI in reusable object

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Alternatively PMI Assembly Filters can also be used to display component level PMI in the context of the assembly.

Re: PMI in reusable object

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Currently a PMI Section View (the term Lightweight was removed in NX 11) view is not a candidate for WAVE PMI Linker. We have plans to support this in a future release.

Highlighted

PMI in reusable object

Valued Contributor
Valued Contributor

Hello, 

 

I would like to define an reusable object with my PMI's is that possible? 

Is there any other way to save an feature with PMI's so i can reuse it? 

 

Thank you

NX 11.0.1.11
NX PMI MBD
NX PMI MBD

This group is dedicated to the topics of PMI (product and manufacturing information) and MBD (model-based definition) in NX.

If you have a question, please post it in the NX Design Forum.

We also recommend you be a PLM World member, as this group supplements an annual roundtable at PLM Connection.

Members (251)