Cancel
Showing results for 
Search instead for 
Did you mean: 

Restrict model edits to PMI only

Creator
Creator

Does anyone know if there is a way to restrict changes to a .prt file to PMI only. Essentially allow for a "drafter" finish up a model a 3D designer has created without editing any of the geometry?

2 REPLIES

Re: Restrict model edits to PMI only

Enthusiast
Enthusiast

Alexander,

You could create snapshot models of the model in question and run a validation routine to ensure that geometry changes were not made while the draftsman completed his/her work to proper specifications.

Since I work for Elysium, I would just use ASFALIS to complete that process. I do not know if there is a similar function in NX.

I do know that years ago while working on a new design program as a manufacturing planner. (We were supposed to plan manufacturing processes as the designers developed the design models. And we didn’t want to slow down the designers by having them explain themselves as the design progressed. So, our answer was to use APIs to program simple scripts that would compare last week’s design to the progress since then. Then we would update/create any processes required to match the new design.) This is a slightly different scenario than you are looking at, but the differences are found and can be operated on in any manner you desire.

Rich Eckenrode

Highlighted

Re: Restrict model edits to PMI only

Phenom
Phenom
A workflow to do that is similar to the master drafting workflow. Use wave geometry linker to associatively copy the solid body of the part. Add your pmi to that associative copy. The linked body has no features that can be edited but it can be updated when the original changes.

Restrict model edits to PMI only

Creator
Creator

Does anyone know if there is a way to restrict changes to a .prt file to PMI only. Essentially allow for a "drafter" finish up a model a 3D designer has created without editing any of the geometry?

NX PMI MBD
NX PMI MBD

This group is dedicated to the topics of PMI (product and manufacturing information) and MBD (model-based definition) in NX.

If you have a question, please post it in the NX Design Forum.

We also recommend you be a PLM World member, as this group supplements an annual roundtable at PLM Connection.

Members (257)