Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

A Couple of Questions Regarding Post Builder

Experimenter
Experimenter

I have 2 questions concerning customizing a post in post builder.

 

1. I am constantly having to split programs into two becuase my machine cannot handle N Codes that exceed N9999. I would like to change the numbering of the .PU1 and .LST files. As of right now it is posting in increments of five and I would like to change it to increments of 2.

 

2. In the attached file you can see in the page header on the .LST file that the RPM is posting as 0 in the last column even though I am calling out a G96. Also I would like to shift the (X, Z, Feed) column headers to the left so that I can add an RPM column header.

1 REPLY 1

Re: A Couple of Questions Regarding Post Builder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This forum is more for customizing NX itself.

Post questions are better asked in the NX Manufacturing forum

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled