Cancel
Showing results for 
Search instead for 
Did you mean: 

A question on Nx IGES import

Pioneer
Pioneer

 

I would like to import a single patch from Rhino into Nx. At first, I export the patch into IGES in Rhino, and then import it into Nx. But something strange happens. As you can see in the second graph, the single patch is decomposed into several patches. Does anyone know the reason for it? And how to import a patch from Rhino into Nx so that the number of patch keeps same? 

1.PNG2.PNG

11 REPLIES

Re: A question on Nx IGES import

Genius
Genius

I'm having a similar issue importing iges files.

 

Try this

 

Go to file->import>IGES

 

Click on the advanced tab in the Import IGES dialog box

 

Click on the “Automatic sewing of surfaces” check box.

 

My understanding of IGES is that it only contains surface (or patch) information and not how those surfaces should be stitched together

Re: A question on Nx IGES import

Pioneer
Pioneer

Hey, thanks for your reply.

I tried the setting you mention, but one patch imported from Rhino into NX are still cut into several patches. As you can see in the graph below, the imported patch has different control points compared with the original patch in Rhino. 

I think the IGES file can only perserve the geometry of the surface, but it will change the control points of patches.

 

 

T1.PNG

Re: A question on Nx IGES import

Genius
Genius

Try the Fill surface command. I'm using it right now on some iges files.

 

http://community.plm.automation.siemens.com/t5/NX-Design-Knowledge-Base/NX-Quick-Tips-NX-9-Fill-Surf...

 

 

Re: A question on Nx IGES import

Pioneer
Pioneer

Hey, thank you for your reply.

 

I first use "Extract Geometry" command to convert all the surfaces into Nurbs and used fill surface command,trying to merge multi-patches into one patch. but I got a different surface compared with the original one.

As you can see from the graph below, the transpart surface is original patch, the blue one is the result of filling surface. I played around with G0 and G1 continuity, but I still can't get the original geometry.

 

Are there any other way to deal with IGES file? 

T1.PNG

 

 

Re: A question on Nx IGES import

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Out of curiosity...

Why is it so important to end up with 1 patch?

If the NX surfaces match the Rhino surfaces, why can't you use them "as is" (or if need be, sew them together then use the sewn surface)?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: A question on Nx IGES import

Pioneer
Pioneer

I am studying IGA now. I would like to know how does the IGES file work and why in diffrent CAD system, the same IGES file can have different control points for the same surface.

Also control points work as degree of freedom for IGA analysis. It will be great that I can pass a surface from Rhino into NX and keep the same control point.

At the same time , doing IGA analysis on multi-surface is more difficult than single patch surface~

 

 

Re: A question on Nx IGES import

Pioneer
Pioneer

I guess it's a simple surface. As you can in the following graph.

 

T1.PNG

Re: A question on Nx IGES import

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What is the degree of the surface in rhino (in both U and V directions)?

 

I'm not sure the limitations of the IGES format, but perhaps the degree of your surface is more than IGES can handle, so it gets split up.

 

NX is limited to a maximum spline degree of 24, but I've never seen anything over degree 7 used in a production model. Also, a single face can be made of multiple patches. After importing the iges file into NX 9, every face in the resulting model has multiple patches.

Re: A question on Nx IGES import

Pioneer
Pioneer

This is the patch infomation.

The degree in U and V are both 4. (So this is a normal case)

Once the patch is imported into NX, the degree in U and V is still 4, but the position of control point changes and more control points are added. 

Maybe as you have said, in some cases, if a surface is imported into NX, it might be cutted into several patches.

T1.PNG

 

!###################################################################
!#### NURBS-BLOCK ####
!###################################################################
NURBS_PATCH 1 : NURBS_2D
CTRL_PTS = CTRL_PTS_DEF 1
NCTRL = 9
MCTRL = 9
PDEG = 4
QDEG = 4
UKNOT = 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 4.8113303771666702e+00, 9.6226607543333298e+00, 1.4433991131499999e+01, 1.9245321508666699e+01, 2.4056651885833300e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01
VKNOT = 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 0.0000000000000000e+00, 4.8113303771666702e+00, 9.6226607543333298e+00, 1.4433991131499999e+01, 1.9245321508666699e+01, 2.4056651885833300e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01, 2.8867982262999998e+01
TRIMMING = B_REP 1
!===================================================================

!###################################################################
!#### TRIMMING ####
!###################################################################
B_REP 1
B_REP_LOOP 1 0 1 TRUE 2 TRUE 3 TRUE
!###################################################################
!#### NURBS-BLOCK-PARAMETER ####
!###################################################################
NURBS_PATCH_PAR 1 : NURBS_1D
CTRL_PTS = CTRL_PTS_PAR 1
NCTRL = 21
PDEG = 3
UKNOT = -1.1944018458043600e+02, -1.1944018458043600e+02, -1.1944018458043600e+02, -1.1944018458043600e+02, -1.1507407394654309e+02, -1.1507407394654309e+02, -1.1507407394654309e+02, -1.0895353069645050e+02, -1.0895353069645050e+02, -1.0895353069645050e+02, -1.0275688009737389e+02, -1.0275688009737389e+02, -1.0275688009737389e+02, -1.0246282033976320e+02, -1.0246282033976320e+02, -1.0246282033976320e+02, -9.8967454139159983e+01, -9.8967454139159983e+01, -9.8967454139159983e+01, -9.5222173308466012e+01, -9.5222173308466012e+01, -9.5222173308466012e+01, -9.2391773860739448e+01, -9.2391773860739448e+01, -9.2391773860739448e+01, -9.2391773860739448e+01
!===================================================================
CTRL_PTS_PAR 1
CTRLPT_PAR_ID 1
CTRLPT_PAR_ID 2
CTRLPT_PAR_ID 3
CTRLPT_PAR_ID 4
CTRLPT_PAR_ID 5
CTRLPT_PAR_ID 6
CTRLPT_PAR_ID 7
CTRLPT_PAR_ID 8
CTRLPT_PAR_ID 9
CTRLPT_PAR_ID 10
CTRLPT_PAR_ID 11
CTRLPT_PAR_ID 12
CTRLPT_PAR_ID 13
CTRLPT_PAR_ID 14
CTRLPT_PAR_ID 15
CTRLPT_PAR_ID 16
CTRLPT_PAR_ID 17
CTRLPT_PAR_ID 18
CTRLPT_PAR_ID 19
CTRLPT_PAR_ID 20
CTRLPT_PAR_ID 21
CTRLPT_PAR_ID 22
!===================================================================
!###################################################################
!#### NURBS-BLOCK-PARAMETER ####
!###################################################################
NURBS_PATCH_PAR 2 : NURBS_1D
CTRL_PTS = CTRL_PTS_PAR 2
NCTRL = 256
PDEG = 4
UKNOT = 4.1256653737248691e+01, 4.1256653737248691e+01, 4.1256653737248691e+01, 4.1256653737248691e+01, 4.1256653737248691e+01, 4.1868112950087223e+01, 4.1868112950087223e+01, 4.1868112950087223e+01, 4.1868112950087223e+01, 4.2525950948599558e+01, 4.2525950948599558e+01, 4.2525950948599558e+01, 4.2525950948599558e+01, 4.3183788947111907e+01, 4.3183788947111907e+01, 4.3183788947111907e+01, 4.3183788947111907e+01, 4.3820188768558701e+01, 4.3820188768558701e+01, 4.3820188768558701e+01, 4.3820188768558701e+01, 4.4456588590005467e+01, 4.4456588590005467e+01, 4.4456588590005467e+01, 4.4456588590005467e+01, 4.5092988411452239e+01, 4.5092988411452239e+01, 4.5092988411452239e+01, 4.5092988411452239e+01, 4.5729388232899012e+01, 4.5729388232899012e+01, 4.5729388232899012e+01, 4.5729388232899012e+01, 4.6387226231411361e+01, 4.6387226231411361e+01, 4.6387226231411361e+01, 4.6387226231411361e+01, 4.7045064229923717e+01, 4.7045064229923717e+01, 4.7045064229923717e+01, 4.7045064229923717e+01, 4.7722460275495912e+01, 4.7722460275495912e+01, 4.7722460275495912e+01, 4.7722460275495912e+01, 4.8399856321068093e+01, 4.8399856321068093e+01, 4.8399856321068093e+01, 4.8399856321068093e+01, 4.9094460614692913e+01, 4.9094460614692913e+01, 4.9094460614692913e+01, 4.9094460614692913e+01, 4.9789064908317727e+01, 4.9789064908317727e+01, 4.9789064908317727e+01, 4.9789064908317727e+01, 5.1219256964192752e+01, 5.1219256964192752e+01, 5.1219256964192752e+01, 5.1219256964192752e+01, 5.2649449020067763e+01, 5.2649449020067763e+01, 5.2649449020067763e+01, 5.2649449020067763e+01, 5.4110092412535927e+01, 5.4110092412535927e+01, 5.4110092412535927e+01, 5.4110092412535927e+01, 5.5570735805004098e+01, 5.5570735805004098e+01, 5.5570735805004098e+01, 5.5570735805004098e+01, 5.7031379197472283e+01, 5.7031379197472283e+01, 5.7031379197472283e+01, 5.7031379197472283e+01, 5.8492022589940433e+01, 5.8492022589940433e+01, 5.8492022589940433e+01, 5.8492022589940433e+01, 5.9922214646315453e+01, 5.9922214646315453e+01, 5.9922214646315453e+01, 5.9922214646315453e+01, 6.1352406702690473e+01, 6.1352406702690473e+01, 6.1352406702690473e+01, 6.1352406702690473e+01, 6.2047010996315286e+01, 6.2047010996315286e+01, 6.2047010996315286e+01, 6.2047010996315286e+01, 6.2741615289940121e+01, 6.2741615289940121e+01, 6.2741615289940121e+01, 6.2741615289940121e+01, 6.3419011335512302e+01, 6.3419011335512302e+01, 6.3419011335512302e+01, 6.3419011335512302e+01, 6.4096407381084475e+01, 6.4096407381084475e+01, 6.4096407381084475e+01, 6.4096407381084475e+01, 6.4754245379596838e+01, 6.4754245379596838e+01, 6.4754245379596838e+01, 6.4754245379596838e+01, 6.5412083378109173e+01, 6.5412083378109173e+01, 6.5412083378109173e+01, 6.5412083378109173e+01, 6.6048483199555960e+01, 6.6048483199555960e+01, 6.6048483199555960e+01, 6.6048483199555960e+01, 6.6684883021002719e+01, 6.6684883021002719e+01, 6.6684883021002719e+01, 6.6684883021002719e+01, 6.7321282842449506e+01, 6.7321282842449506e+01, 6.7321282842449506e+01, 6.7321282842449506e+01, 6.7957682663896293e+01, 6.7957682663896293e+01, 6.7957682663896293e+01, 6.7957682663896293e+01, 6.8615520662408628e+01, 6.8615520662408628e+01, 6.8615520662408628e+01, 6.8615520662408628e+01, 6.9273358660920991e+01, 6.9273358660920991e+01, 6.9273358660920991e+01, 6.9273358660920991e+01, 6.9950754706493171e+01, 6.9950754706493171e+01, 6.9950754706493171e+01, 6.9950754706493171e+01, 7.0628150752065352e+01, 7.0628150752065352e+01, 7.0628150752065352e+01, 7.0628150752065352e+01, 7.1322755045690172e+01, 7.1322755045690172e+01, 7.1322755045690172e+01, 7.1322755045690172e+01, 7.2017359339314993e+01, 7.2017359339314993e+01, 7.2017359339314993e+01, 7.2017359339314993e+01, 7.3447551395190018e+01, 7.3447551395190018e+01, 7.3447551395190018e+01, 7.3447551395190018e+01, 7.4877743451065029e+01, 7.4877743451065029e+01, 7.4877743451065029e+01, 7.4877743451065029e+01, 7.6338386843533186e+01, 7.6338386843533186e+01, 7.6338386843533186e+01, 7.6338386843533186e+01, 7.7799030236001371e+01, 7.7799030236001371e+01, 7.7799030236001371e+01, 7.7799030236001371e+01, 7.9259673628469528e+01, 7.9259673628469528e+01, 7.9259673628469528e+01, 7.9259673628469528e+01, 8.0720317020937713e+01, 8.0720317020937713e+01, 8.0720317020937713e+01, 8.0720317020937713e+01, 8.2150509077312719e+01, 8.2150509077312719e+01, 8.2150509077312719e+01, 8.2150509077312719e+01, 8.3580701133687739e+01, 8.3580701133687739e+01, 8.3580701133687739e+01, 8.3580701133687739e+01, 8.4275305427312574e+01, 8.4275305427312574e+01, 8.4275305427312574e+01, 8.4275305427312574e+01, 8.4969909720937395e+01, 8.4969909720937395e+01, 8.4969909720937395e+01, 8.4969909720937395e+01, 8.5647305766509561e+01, 8.5647305766509561e+01, 8.5647305766509561e+01, 8.5647305766509561e+01, 8.6324701812081742e+01, 8.6324701812081742e+01, 8.6324701812081742e+01, 8.6324701812081742e+01, 8.6982539810594091e+01, 8.6982539810594091e+01, 8.6982539810594091e+01, 8.6982539810594091e+01, 8.7640377809106468e+01, 8.7640377809106468e+01, 8.7640377809106468e+01, 8.7640377809106468e+01, 8.8276777630553227e+01, 8.8276777630553227e+01, 8.8276777630553227e+01, 8.8276777630553227e+01, 8.8913177451999999e+01, 8.8913177451999999e+01, 8.8913177451999999e+01, 8.8913177451999999e+01, 8.9549577288506441e+01, 8.9549577288506441e+01, 8.9549577288506441e+01, 8.9549577288506441e+01, 9.0185977125012869e+01, 9.0185977125012869e+01, 9.0185977125012869e+01, 9.0185977125012869e+01, 9.0843815138993889e+01, 9.0843815138993889e+01, 9.0843815138993889e+01, 9.0843815138993889e+01, 9.1501653152974896e+01, 9.1501653152974896e+01, 9.1501653152974896e+01, 9.1501653152974896e+01, 9.2179049214680091e+01, 9.2179049214680091e+01, 9.2179049214680091e+01, 9.2179049214680091e+01, 9.2856445276385287e+01, 9.2856445276385287e+01, 9.2856445276385287e+01, 9.2856445276385287e+01, 9.3551049586451683e+01, 9.3551049586451683e+01, 9.3551049586451683e+01, 9.3551049586451683e+01, 9.4245653896518078e+01, 9.4245653896518078e+01, 9.4245653896518078e+01, 9.4245653896518078e+01, 9.5675845986799303e+01, 9.5675845986799303e+01, 9.5675845986799303e+01, 9.5675845986799303e+01, 9.7106038077080512e+01, 9.7106038077080512e+01, 9.7106038077080512e+01, 9.7106038077080512e+01, 9.7900192950862561e+01, 9.7900192950862561e+01, 9.7900192950862561e+01, 9.7900192950862561e+01, 9.7900192950862561e+01
!===================================================================
CTRL_PTS_PAR 2
CTRLPT_PAR_ID 23
CTRLPT_PAR_ID 24
CTRLPT_PAR_ID 25
CTRLPT_PAR_ID 26
CTRLPT_PAR_ID 27
CTRLPT_PAR_ID 28
CTRLPT_PAR_ID 29
CTRLPT_PAR_ID 30
CTRLPT_PAR_ID 31
CTRLPT_PAR_ID 32
CTRLPT_PAR_ID 33
CTRLPT_PAR_ID 34
CTRLPT_PAR_ID 35
CTRLPT_PAR_ID 36
CTRLPT_PAR_ID 37
CTRLPT_PAR_ID 38
CTRLPT_PAR_ID 39
CTRLPT_PAR_ID 40
CTRLPT_PAR_ID 41
CTRLPT_PAR_ID 42
CTRLPT_PAR_ID 43
CTRLPT_PAR_ID 44
CTRLPT_PAR_ID 45
CTRLPT_PAR_ID 46
CTRLPT_PAR_ID 47
CTRLPT_PAR_ID 48
CTRLPT_PAR_ID 49
CTRLPT_PAR_ID 50
CTRLPT_PAR_ID 51
CTRLPT_PAR_ID 52
CTRLPT_PAR_ID 53
CTRLPT_PAR_ID 54
CTRLPT_PAR_ID 55
CTRLPT_PAR_ID 56
CTRLPT_PAR_ID 57
CTRLPT_PAR_ID 58
CTRLPT_PAR_ID 59
CTRLPT_PAR_ID 60
CTRLPT_PAR_ID 61
CTRLPT_PAR_ID 62
CTRLPT_PAR_ID 63
CTRLPT_PAR_ID 64
CTRLPT_PAR_ID 65
CTRLPT_PAR_ID 66
CTRLPT_PAR_ID 67
CTRLPT_PAR_ID 68
CTRLPT_PAR_ID 69
CTRLPT_PAR_ID 70
CTRLPT_PAR_ID 71
CTRLPT_PAR_ID 72
CTRLPT_PAR_ID 73
CTRLPT_PAR_ID 74
CTRLPT_PAR_ID 75
CTRLPT_PAR_ID 76
CTRLPT_PAR_ID 77
CTRLPT_PAR_ID 78
CTRLPT_PAR_ID 79
CTRLPT_PAR_ID 80
CTRLPT_PAR_ID 81
CTRLPT_PAR_ID 82
CTRLPT_PAR_ID 83
CTRLPT_PAR_ID 84
CTRLPT_PAR_ID 85
CTRLPT_PAR_ID 86
CTRLPT_PAR_ID 87
CTRLPT_PAR_ID 88
CTRLPT_PAR_ID 89
CTRLPT_PAR_ID 90
CTRLPT_PAR_ID 91
CTRLPT_PAR_ID 92
CTRLPT_PAR_ID 93
CTRLPT_PAR_ID 94
CTRLPT_PAR_ID 95
CTRLPT_PAR_ID 96
CTRLPT_PAR_ID 97
CTRLPT_PAR_ID 98
CTRLPT_PAR_ID 99
CTRLPT_PAR_ID 100
CTRLPT_PAR_ID 101
CTRLPT_PAR_ID 102
CTRLPT_PAR_ID 103
CTRLPT_PAR_ID 104
CTRLPT_PAR_ID 105
CTRLPT_PAR_ID 106
CTRLPT_PAR_ID 107
CTRLPT_PAR_ID 108
CTRLPT_PAR_ID 109
CTRLPT_PAR_ID 110
CTRLPT_PAR_ID 111
CTRLPT_PAR_ID 112
CTRLPT_PAR_ID 113
CTRLPT_PAR_ID 114
CTRLPT_PAR_ID 115
CTRLPT_PAR_ID 116
CTRLPT_PAR_ID 117
CTRLPT_PAR_ID 118
CTRLPT_PAR_ID 119
CTRLPT_PAR_ID 120
CTRLPT_PAR_ID 121
CTRLPT_PAR_ID 122
CTRLPT_PAR_ID 123
CTRLPT_PAR_ID 124
CTRLPT_PAR_ID 125
CTRLPT_PAR_ID 126
CTRLPT_PAR_ID 127
CTRLPT_PAR_ID 128
CTRLPT_PAR_ID 129
CTRLPT_PAR_ID 130
CTRLPT_PAR_ID 131
CTRLPT_PAR_ID 132
CTRLPT_PAR_ID 133
CTRLPT_PAR_ID 134
CTRLPT_PAR_ID 135
CTRLPT_PAR_ID 136
CTRLPT_PAR_ID 137
CTRLPT_PAR_ID 138
CTRLPT_PAR_ID 139
CTRLPT_PAR_ID 140
CTRLPT_PAR_ID 141
CTRLPT_PAR_ID 142
CTRLPT_PAR_ID 143
CTRLPT_PAR_ID 144
CTRLPT_PAR_ID 145
CTRLPT_PAR_ID 146
CTRLPT_PAR_ID 147
CTRLPT_PAR_ID 148
CTRLPT_PAR_ID 149
CTRLPT_PAR_ID 150
CTRLPT_PAR_ID 151
CTRLPT_PAR_ID 152
CTRLPT_PAR_ID 153
CTRLPT_PAR_ID 154
CTRLPT_PAR_ID 155
CTRLPT_PAR_ID 156
CTRLPT_PAR_ID 157
CTRLPT_PAR_ID 158
CTRLPT_PAR_ID 159
CTRLPT_PAR_ID 160
CTRLPT_PAR_ID 161
CTRLPT_PAR_ID 162
CTRLPT_PAR_ID 163
CTRLPT_PAR_ID 164
CTRLPT_PAR_ID 165
CTRLPT_PAR_ID 166
CTRLPT_PAR_ID 167
CTRLPT_PAR_ID 168
CTRLPT_PAR_ID 169
CTRLPT_PAR_ID 170
CTRLPT_PAR_ID 171
CTRLPT_PAR_ID 172
CTRLPT_PAR_ID 173
CTRLPT_PAR_ID 174
CTRLPT_PAR_ID 175
CTRLPT_PAR_ID 176
CTRLPT_PAR_ID 177
CTRLPT_PAR_ID 178
CTRLPT_PAR_ID 179
CTRLPT_PAR_ID 180
CTRLPT_PAR_ID 181
CTRLPT_PAR_ID 182
CTRLPT_PAR_ID 183
CTRLPT_PAR_ID 184
CTRLPT_PAR_ID 185
CTRLPT_PAR_ID 186
CTRLPT_PAR_ID 187
CTRLPT_PAR_ID 188
CTRLPT_PAR_ID 189
CTRLPT_PAR_ID 190
CTRLPT_PAR_ID 191
CTRLPT_PAR_ID 192
CTRLPT_PAR_ID 193
CTRLPT_PAR_ID 194
CTRLPT_PAR_ID 195
CTRLPT_PAR_ID 196
CTRLPT_PAR_ID 197
CTRLPT_PAR_ID 198
CTRLPT_PAR_ID 199
CTRLPT_PAR_ID 200
CTRLPT_PAR_ID 201
CTRLPT_PAR_ID 202
CTRLPT_PAR_ID 203
CTRLPT_PAR_ID 204
CTRLPT_PAR_ID 205
CTRLPT_PAR_ID 206
CTRLPT_PAR_ID 207
CTRLPT_PAR_ID 208
CTRLPT_PAR_ID 209
CTRLPT_PAR_ID 210
CTRLPT_PAR_ID 211
CTRLPT_PAR_ID 212
CTRLPT_PAR_ID 213
CTRLPT_PAR_ID 214
CTRLPT_PAR_ID 215
CTRLPT_PAR_ID 216
CTRLPT_PAR_ID 217
CTRLPT_PAR_ID 218
CTRLPT_PAR_ID 219
CTRLPT_PAR_ID 220
CTRLPT_PAR_ID 221
CTRLPT_PAR_ID 222
CTRLPT_PAR_ID 223
CTRLPT_PAR_ID 224
CTRLPT_PAR_ID 225
CTRLPT_PAR_ID 226
CTRLPT_PAR_ID 227
CTRLPT_PAR_ID 228
CTRLPT_PAR_ID 229
CTRLPT_PAR_ID 230
CTRLPT_PAR_ID 231
CTRLPT_PAR_ID 232
CTRLPT_PAR_ID 233
CTRLPT_PAR_ID 234
CTRLPT_PAR_ID 235
CTRLPT_PAR_ID 236
CTRLPT_PAR_ID 237
CTRLPT_PAR_ID 238
CTRLPT_PAR_ID 239
CTRLPT_PAR_ID 240
CTRLPT_PAR_ID 241
CTRLPT_PAR_ID 242
CTRLPT_PAR_ID 243
CTRLPT_PAR_ID 244
CTRLPT_PAR_ID 245
CTRLPT_PAR_ID 246
CTRLPT_PAR_ID 247
CTRLPT_PAR_ID 248
CTRLPT_PAR_ID 249
CTRLPT_PAR_ID 250
CTRLPT_PAR_ID 251
CTRLPT_PAR_ID 252
CTRLPT_PAR_ID 253
CTRLPT_PAR_ID 254
CTRLPT_PAR_ID 255
CTRLPT_PAR_ID 256
CTRLPT_PAR_ID 257
CTRLPT_PAR_ID 258
CTRLPT_PAR_ID 259
CTRLPT_PAR_ID 260
CTRLPT_PAR_ID 261
CTRLPT_PAR_ID 262
CTRLPT_PAR_ID 263
CTRLPT_PAR_ID 264
CTRLPT_PAR_ID 265
CTRLPT_PAR_ID 266
CTRLPT_PAR_ID 267
CTRLPT_PAR_ID 268
CTRLPT_PAR_ID 269
CTRLPT_PAR_ID 270
CTRLPT_PAR_ID 271
CTRLPT_PAR_ID 272
CTRLPT_PAR_ID 273
CTRLPT_PAR_ID 274
CTRLPT_PAR_ID 275
CTRLPT_PAR_ID 276
CTRLPT_PAR_ID 277
CTRLPT_PAR_ID 278
CTRLPT_PAR_ID 279
!===================================================================
!###################################################################
!#### NURBS-BLOCK-PARAMETER ####
!###################################################################
NURBS_PATCH_PAR 3 : NURBS_1D
CTRL_PTS = CTRL_PTS_PAR 3
NCTRL = 27
PDEG = 3
UKNOT = -6.5258567255432837e+01, -6.5258567255432837e+01, -6.5258567255432837e+01, -6.5258567255432837e+01, -5.9696263799717173e+01, -5.9696263799717173e+01, -5.9696263799717173e+01, -5.8377045772679487e+01, -5.8377045772679487e+01, -5.8377045772679487e+01, -5.6151357427952632e+01, -5.6151357427952632e+01, -5.6151357427952632e+01, -5.2458771876371557e+01, -5.2458771876371557e+01, -5.2458771876371557e+01, -4.7751960674418910e+01, -4.7751960674418910e+01, -4.7751960674418910e+01, -4.6996637593732693e+01, -4.6996637593732693e+01, -4.6996637593732693e+01, -3.6154406196182777e+01, -3.6154406196182777e+01, -3.6154406196182777e+01, -3.5446615821509873e+01, -3.5446615821509873e+01, -3.5446615821509873e+01, -2.7206591734788059e+01, -2.7206591734788059e+01, -2.7206591734788059e+01, -2.7206591734788059e+01
!===================================================================
CTRL_PTS_PAR 3
CTRLPT_PAR_ID 280
CTRLPT_PAR_ID 281
CTRLPT_PAR_ID 282
CTRLPT_PAR_ID 283
CTRLPT_PAR_ID 284
CTRLPT_PAR_ID 285
CTRLPT_PAR_ID 286
CTRLPT_PAR_ID 287
CTRLPT_PAR_ID 288
CTRLPT_PAR_ID 289
CTRLPT_PAR_ID 290
CTRLPT_PAR_ID 291
CTRLPT_PAR_ID 292
CTRLPT_PAR_ID 293
CTRLPT_PAR_ID 294
CTRLPT_PAR_ID 295
CTRLPT_PAR_ID 296
CTRLPT_PAR_ID 297
CTRLPT_PAR_ID 298
CTRLPT_PAR_ID 299
CTRLPT_PAR_ID 300
CTRLPT_PAR_ID 301
CTRLPT_PAR_ID 302
CTRLPT_PAR_ID 303
CTRLPT_PAR_ID 304
CTRLPT_PAR_ID 305
CTRLPT_PAR_ID 306
CTRLPT_PAR_ID 307
!===================================================================
!===================================================================