Cancel
Showing results for 
Search instead for 
Did you mean: 

AFU record: GetComplexData ?

Gears Phenom Gears Phenom
Gears Phenom

To all

 

I am trying to retrieve the Y data from a complex (afu) record; that is a record with Real and imaginary as Y values.

I am using the code below to extract the values but I only get hte Real part in the array theYvalues?

 

Dim theXvalues(),theYvalues() As Double
myAfuData.GetComplexData(theXvalues, theYvalues)

 

how do I get the imaginary part too? I ultimately need to calculate the magnitude

 

Thanks

Regards

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
3 REPLIES

Re: AFU record: GetComplexData ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Dim theXvalues(),theYvalues(), imaginary() As Double
imaginary = myAfuData.GetComplexData(theXvalues, theYvalues)

Re: AFU record: GetComplexData ?

Gears Phenom Gears Phenom
Gears Phenom

Dhoo. So obvious now that you showed me!

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: AFU record: GetComplexData ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Unfortunately, the signature of this function is a bit convoluted. The imaginary/phase values are returned by the function, so you really need to call it like:

 

Dim theXvalues(),theRealMagValues(),theImagPhaseValues() As Double
theImagPhaseValues = myAfuData.GetComplexData(theXvalues, theRealMagValues)

 

 

Public Function GetComplexData(ByRef xValues() As Double, ByRef yValues() As Double) As Double()
     Member of NXOpen.CAE.AfuData
Summary:
Get the XY data of an AFU Data Record when the ordinate type is Complex

Parameters:
xValues: Abscissa element data values
yValues: Ordinate element data values for real part or magnitude part

Return Values:
Ordinate element data values for imaginary part or phase part

Remarks:
Created in NX4.0.0
License requirements: nx_ftk ("NX Advanced Graphing")