Cancel
Showing results for 
Search instead for 
Did you mean: 

Access UF from NX OPEN - JAVA

Creator
Creator

Hi there,

how can I use

UF_PS_export_linked_data

within JAVA ?

 

Right now I am using

UF_PS_export_data

with

    nxopen.UFSession ufs = (nxopen.UFSession)nxopen.SessionFactory.get("UFSession");

    ufs.ps().exportData(myTs, xt_file_path);

 

However there does not seem to be a JAVA implementation for export_linked_data which I need to use in order to set a parasolid version for export.

 

Thanks in advance !

2 REPLIES

Re: Access UF from NX OPEN - JAVA

Phenom
Phenom

Some UF functions are not wrapped in NXOpen because they contain unions which do not translate well.

However, UF_PS_export_linked_data() does not seem to reference any unions, so it should be wrapped I would have thought. It looks like this is an omission.

Your best bet is to open and IR with GTAC.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: NX8.5.3.3 MP11 64bit Testing: NX9.0.2.5

Re: Access UF from NX OPEN - JAVA

Genius
Genius

In the NX API documentation, there is a list of "Non-wrapped NX Open C functions"

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api/#uid:xid1162445:index_nxopen_prog_guide:id...

but the function UF_PS_export_linked_data is not listed.

 

Either the documentation is wrong or, like Graham already told you, this is a Siemens omission.

I also recommend you to contact GTAC.