Cancel
Showing results for 
Search instead for 
Did you mean: 

Add objects to the model

Creator
Creator

Hi everyone!

 

Is there an analogue of the Delete List, but to add objects to the model? If not, what would be the way to go? Thank you.

 

Regards.

 

P.S. by the delete list I mean the one that is used here: theSession.UpdateManager.AddToDeleteList(obj);

 

2 REPLIES

Re: Add objects to the model

Honored Contributor
Honored Contributor

To add objects to a file, they either need to be created in the file, or imported from a different file (or, similarly, exported from another file to the target file).

Re: Add objects to the model

Esteemed Contributor
Esteemed Contributor

Why are you asking this?

What are you trying to achieve?

 

When you create objects, they get created.  No need to add to a list to create "again"

 

The issue with deletion (or at least one of them) is when looping thru objects, and picking some to delete, you can't delete them while you are in the loop (it hoses up the looping).  So you add items to a "delete list" in the loop, then (when the loop is done), delete them.

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled