Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding bodies to Kinematic Configurator

Creator
Creator

Hello everyone,

 

I am trying to add bodies to the tool-nocut-component in the machine tool builder.

I started recording a journal to get a rough overview what is needed.

Everything works fine so far, i just have a problem in understanding the behaviour of:

kinematicComponentBuilder1.AddGeometry(body1)

I have two bodies which I want to identify by name, because they are both named "NOCUT".

When I record the journal this code is the result:

Dim body1 As Body = CType(workPart.Bodies.FindObject("UNPARAMETERIZED_FEATURE(3)"), Body)

kinematicComponentBuilder1.AddGeometry(body1)

Dim body2 As Body = CType(workPart.Bodies.FindObject("UNPARAMETERIZED_FEATURE(1)"), Body)

kinematicComponentBuilder1.AddGeometry(body2)

This will result in showing two bodies when selecting the non_cutting part in the machine tool builder

 

I changed to code to cycle through all bodies with the name "NOCUT":

For Each bbody As Body In theSession.Parts.Work.Bodies
            Dim aBodyTag As Tag = Tag.Null
            theUfSession.Obj.CycleByNameAndType(displayPart.Tag, "NOCUT", UFConstants.UF_solid_type, True, aBodyTag)
            If Not aBodyTag = Tag.Null Then
                BodyNoCut = CType(theSession.GetObjectManager().GetTaggedObject(aBodyTag), Body)
                NoCutKinCompBuild.AddGeometry(BodyNoCut)
            Else
                Exit Sub
            End If
        Next

This will result in showing one body when selecting the non_cutting part in the machine tool builder,

but it will show the correct two bodies when i am retrieving the tool from the database in CAM.

 

Shouldn't be the result the same? And if not, how can I change to code to display the selected parts correctly in the machine tool builder?

 

Thanks for your help!

2 REPLIES

Re: Adding bodies to Kinematic Configurator

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1) I would report to GTAC - it may be a bug if both bodies have the same name

 

2) I would try a test - try naming the bodies "NOCUT1", "NOCUT2", etc.
Then loop thru, but build the name to search for on-the-fly, and add them.  - see if this works better.

 

if (2) works correctly, you have a solution (maybe not one you want, but it is a solution)

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Adding bodies to Kinematic Configurator

Creator
Creator

Hello,

 

I just made this test, I renamed all the bodies to NOCUT0, NOCUT1 etc. in the same loop, just before adding them. Now both bodies will be shown if I select the NON_CUTTING part at the machine tool builder.

 

Good Idea! Haven't thought about rename.

Thanks alot!