Cancel
Showing results for 
Search instead for 
Did you mean: 

Annotation to user defined object in NXOpen

Can we add user defined annotation to "UDO Feature" as shown in attached image?? 

 

If yes can we control edit of annotation through callback???

5 REPLIES

Re: Annotation to user defined object in NXOpen

Esteemed Contributor
Esteemed Contributor

Note that drafting text (and I am assuming PMI text) can include references to expressions, so if you want the "value" text to change as the feature is changed, the answer should be yes.

If (depending on UDO changes) lines of text need to be added/removed, that can probably be done, but it will require code.

 

If that is not what you are asking about, please try to explain better.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Annotation to user defined object in NXOpen

thanks for reply...

Can you please explain with small prototype....

Assume that you have point as udo and annotations should be like attached image...

Re: Annotation to user defined object in NXOpen

how to create tabular note of PMI dimensions in model

Re: Annotation to user defined object in NXOpen

Pioneer
Pioneer

Hi

The below code will help you to Create PMI table in model file. :-

 

UFTabnot.SectionPrefs secPrefs = default(UFTabnot.SectionPrefs);
ufs.Tabnot.AskDefaultSectionPrefs(out secPrefs);
ufs.Tabnot.Create(ref secPrefs, origin, out tabnotelocation);

 

After This you can edit each cell of the table.

 

Thanks

Gunjeet

Re: Annotation to user defined object in NXOpen

Thanks for your quick answer.

Is it possible to draw tabular note should be always in current view?