cancel
Showing results for 
Search instead for 
Did you mean: 

Attributes all titles from category (VB.NET)

Creator
Creator

Hello,

 

I'm looking for an  answer in VB.NET

I have a part with some attributes I put under one specific category, named "LCA"
Is there a way to get all the titles under this category as a string()?

 

Thanks in advance,

Laurens

Student at University of Ghent

 

6 REPLIES

Re: Attributes all titles from category (VB.NET)

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Since the Category designator is held in a structure element in the AttributeInformation, I think you would need to get all of the part attributes with GetUserAttributes(), and then iterate through them to see if each one is marked with the Category that you are interested in.  (I have not tested this.)

 

Re: Attributes all titles from category (VB.NET)

Creator
Creator
This was indeed the solution.
Thanks!

Below the code that worked for me:

Dim attributeList As NXObject.AttributeInformation() = workPart.GetUserAttributes()
Dim titleList As New List(Of String)()

For Each att As NXObject.AttributeInformation In attributeList
If att.Category.Equals("CategoryName") Then
titleList.Add(att.Title.ToString)

End If
Next

Re: Attributes all titles from category (VB.NET)

Siemens Phenom Siemens Phenom
Siemens Phenom

Try this:

 

Option Strict Off
Imports System
Imports NXOpen
Imports NXOpen.NXObject
Imports NXOpen.UF

Module get_all_titles_in_a_specified_part_attribute_category

    Dim theSession As Session = Session.GetSession()

    Sub Main()

        Dim wp As Part = theSession.Parts.Work
        Dim specifiedCategory As String = "LCA"

        Dim allPartAttrInfos() As AttributeInformation = wp.GetUserAttributes()

        For Each thisAttrInfo In allPartAttrInfos
            If thisAttrInfo.Category.Equals("LCA") Then

                Echo("Title: " & thisAttrInfo.Title.ToString())
                Echo("    Value: " & thisAttrInfo.StringValue.ToString())
                Echo("    Category: " & thisAttrInfo.Category.ToString())
                Echo(" ")
            End If
        Next

    End Sub

    Sub Echo(ByVal output As String)

        theSession.ListingWindow.Open()
        theSession.ListingWindow.WriteLine(output)
        theSession.LogFile.WriteLine(output)

    End Sub

    Public Function GetUnloadOption(ByVal dummy As String) As Integer
        Return Session.LibraryUnloadOption.Immediately
    End Function

End Module

Re: Attributes all titles from category (VB.NET)

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm glad you got it to work - I think we were posting simultaneously.  8-)

 

Re: Attributes all titles from category (VB.NET)

Creator
Creator

Yes, I think so too.
Thank you for your help. Smiley Happy
May I ask what "Echo" does in your code? I'm not familiar with that command.

Re: Attributes all titles from category (VB.NET)

Siemens Phenom Siemens Phenom
Siemens Phenom

It is a very small subroutine that is used to send the output to both the information window and the NX syslog.  You will see it in a lot of the example programs that we post on the Solution Center.