Cancel
Showing results for 
Search instead for 
Did you mean: 

Block UI Styler error

Experimenter
Experimenter

Hallo !!

 

i am working with (Block UI Styler )and i get this error :
Error Number: 943006

 

the picture is taken from the log file!

 

errorrr.png

 

1 REPLY

Re: Block UI Styler error

Gears Phenom Gears Phenom
Gears Phenom

not sure but check that you are using the same name GUI vs. code

for example on the GUI if you have inserted a toggle and called it  'mytoggle' make sure that you are usind this name in the code.

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)