Cancel
Showing results for 
Search instead for 
Did you mean: 

BlockStyler Curve Collector Block Cursor Position required to find end points closer

Pioneer
Pioneer

 

Hi,

 

Im trying to find the end point which is closer to the selected pick point on a curve.

 

How to fetch the pick point i.e cursor position from curve collector UIBlock, i did not found any method to get the same like SelectObject UIBlock has Pick Point option.

 

is there any other alternative way to get the cursor position selected on curve.

 

 

Regards,

Maddy

Windows 7 x64
NX 8.5, NX 9.0. And also NX 7.5
Visual Studio 2010 SP1, 2012 Update 4
2 REPLIES

Re: BlockStyler Curve Collector Block Cursor Position required to find end points closer

Siemens Phenom Siemens Phenom
Siemens Phenom

In NX9 (at least), the SelectObject block has a PickPoint property.

山田
yamada

Re: BlockStyler Curve Collector Block Cursor Position required to find end points closer

Pioneer
Pioneer

 

 

Hi Yamda,

 

Im trying to find the pick point with UIBlock CURVECOLLECTOR not with Select Object.

 

Regards,

Maddy

Windows 7 x64
NX 8.5, NX 9.0. And also NX 7.5
Visual Studio 2010 SP1, 2012 Update 4