Cancel
Showing results for 
Search instead for 
Did you mean: 

[CAM] How to flip material side in Surface Area Drive Method in Fixed Contour Operation ?

Experimenter
Experimenter

Dears,

 

    I'm using NXopenC++ to create a fixed contour operation, the drive method of the operation is Surface Area, it is easy for me to append a face to the Specify Drive Geometry, However, I can't change the material side which is automatically setted by NX.

Though I can find the function in library which meets my needs, but it does not work..

 

Is there any suggestion?

fun.png

 

 

 

 

 

 

 

 

 

cam问题 - 副本.png

 

 

1 REPLY

Re: [CAM] How to flip material side in Surface Area Drive Method in Fixed Contour Operation ?

Experimenter
Experimenter

Finally, I found the answer of this question.

It's all about the NX version of the [cam template part].

 

fun.png

 

at first, I use the lower version NX part to establish a [cam template part] ,the part may be lower than NX8.0.

As indicted by the function declaration, only the part which version higher than 8.0 could use FlipMaterial()

 

At last, i rebulid the [cam template part] by Nx10.0, and the funs work!!