Cancel
Showing results for 
Search instead for 
Did you mean: 

CLF Output Setting

Pioneer
Pioneer

Hello Guys

I use NX10 to mill a chamfer with ZLevel. Then I output CL file that is ok.(CLSF Output with decimal 4). After I change to decimal 7. CL file is more CIRCLE line out (Tape file G3) that is wrong. I do not know where is wrong?

Thanks!

Kevin

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
2 REPLIES

Re: CLF Output Setting

Esteemed Contributor
Esteemed Contributor

I would not say that it is wrong, it is just better to use more decimal places to get a better tool path.

A circle is smoother than consecutive lines.

If you don't like circles, change the output of the operation to linear.

Do not change the post-processor to only output linear motion, since then you get facets instead of smooth circular moves.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: CLF Output Setting

This forum for customization and API programming. 

If this question is about NC programming, I would ask it in the Manufacturing forum.

Mark Rief
Retired Siemens