Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Can I use MenuScript to add a PRE action to a button that is defined in a TBR file?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The reuse library is divided into multiple sections, one is the tree, which only lists the structure, the contained items are listed in the members panel below.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Can I use MenuScript to add a PRE action to a button that is defined in a TBR file?

Gears Phenom Gears Phenom
Gears Phenom

Oh, I see, duh Robot Frustrated

I think this could sort it out actually. I just have to convince the guys that organise the setup of the NX servers to implement this so UDFs are accessed via the ReUse instead of Insert->User Defined.

Just one question, how would you set this in the UGII_ENV.DAT? I could trawl through it, but I'm being lazy Robot wink

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: Can I use MenuScript to add a PRE action to a button that is defined in a TBR file?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How do you specify your environment?

 

I use the Windows environment variable UGII_ENV_FILE to point to a central ugii_env.dat file and specify a custom variable there.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide