Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Open Help in NX 9.0.

Creator
Creator

Capture.JPG

 

hello guys...

i am not to much aware about NX..

please help me to solve above error ...

 

how can i access help of nx ??

 

how can i access API of NX??

 

thanks in advaned....

5 REPLIES

Re: Can't Open Help in NX 9.0.

Hi @Harsh9592,

NX base installation do not include the NX Documentation/NX Help Library. You need to install it on top of the base installation.

You can also refer the online NX documentation here.

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: Can't Open Help in NX 9.0.

Creator
Creator

2.JPG

 

Thanks for your reply..

 

i have another problem that i am downloaded the NX .net API guide but it wasn't opened.

 

as shown in attached photo it was blank..

 

please help me to resolve this problem...

 

thanks in advanced !!

Re: Can't Open Help in NX 9.0.

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

The .NET API reference guide is formatted as a .chm file, which cannot be viewed over a network and must be installed and viewed locally on a system.

NX Design Apps Documentation & Courseware Manager

Re: Can't Open Help in NX 9.0.

Honored Contributor
Honored Contributor

The first time that I downloaded the file and opened it, it was blank. I chalked it up to a download error and deleted the file. The second time I downloaded it, it loaded correctly.

Re: Can't Open Help in NX 9.0.

Valued Contributor
Valued Contributor

Select the chm file in Explorer. Right click, Properties.

Click on the unblock buttion

 

Open the file again