Cancel
Showing results for 
Search instead for 
Did you mean: 

Can the doc server have nx10 and 11 docs installed simutanously?

Valued Contributor
Valued Contributor

Has anyone tried it?  Now that I think of it I do not recall the client env variable being version specific.

NX 12.0.1
2 REPLIES

Re: Can the doc server have nx10 and 11 docs installed simutanously?

Siemens Legend Siemens Legend
Siemens Legend

Yes, you are correct.

The Document server can have different versions of NX documentation installed. 

I presume that Teamcenter will have (or already has) documenation through the Documentation server.

 

The ENV variable of NX only points to the server and port. NX adds the path required to the correct documentation.

 

Regards,

Gerrit Koelewijn

Re: Can the doc server have nx10 and 11 docs installed simutanously?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX and Teamcenter share the same doc server starting with Tc 10.1.4

We have NX and Teamcenter documentation running without any problem, was just installing the Tc docs on the server and pointing the Tc clients to it, nothing more.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide