Cancel
Showing results for 
Search instead for 
Did you mean: 

Change Position of idSymbol wrt the center of the circle

Pioneer
Pioneer

Hello all,

 

In my program an idSymbol is created with a Leader referring to the center of a selected circle on a drafting view. i need to create the id Symbol in a way sothat when the user change the position of the circle in the sketch the idSymbol moves with it. i have tried to make a journal for this process but there is always something wrong.

 

thanks in advance

1 REPLY

Re: Change Position of idSymbol wrt the center of the circle

Legend
Legend

The IDSymbol needs to be attached to an object.  If you can have a point object that is associative to the arc centre then the IDSymbol can be attached to the point object.  Now the circle may be moved and the point and the IDSymbol will update.

 

Frank Swinkels