Cancel
Showing results for 
Search instead for 
Did you mean: 

Change of composite ID when adding more RAM.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I need to upgrade my computer adding more RAM. Do you know if the composite id will change, making the license unusable?

 

Regards

Frank.

 

3 REPLIES

Re: Change of composite ID when adding more RAM.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I doubt that changing RAM will change the CID, since RAM is nothing essential to licensing.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Change of composite ID when adding more RAM.

Legend
Legend

I've replaced ram without licensing issues. 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.1 / Autoform r7 /WorkNC 2018 r2
Testing:nothing.
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Change of composite ID when adding more RAM.

Legend
Legend

Hi,

 

The composite ID is just a combination of MAC-address and hostname.

It has nothing to do with the other hardware in the computer. just the network card.

 

br

Fred