Cancel
Showing results for 
Search instead for 
Did you mean: 

CheckMate - Object Types

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi -

 

I have few question  regarding checkmate (nx8.5).

 

I have created a layer profile , where I parse in some differents object types into the checker:

mqc_check_objects_layers_mapping.dfa.

The object types could be:

UF_datum_plane_type,UF_coordinate_system_type,UF_sketch_type,UF_line_type and others.

 

My question is: If I will check for , say datumplanes om correct layers , the checker also checks the three datum planes in the datum coordinate system. How can I avoid this. Only want to check for datum planes which is single features.

 

Same issue when I check for a curve on correct layer. It also checks for curves into sketches...

I only want to check for curves that not are part of sketch....

 

Anyone faced the same problem ?

 

Lars