Cancel
Showing results for 
Search instead for 
Did you mean: 

Converting a spline to lines and arcs

Innovator
Innovator

Are there any tips or ideas on how to convert a spline into lines and arcs?

 

Not the simplify button.

4 REPLIES

Re: Converting a spline to lines and arcs

Honored Contributor
Honored Contributor

"Not the simplify button."

 

Because that is too easy?  Smiley Happy

Re: Converting a spline to lines and arcs

Innovator
Innovator
I need them to end up tangent

Re: Converting a spline to lines and arcs

Esteemed Contributor
Esteemed Contributor

InternBL wrote:
I need them to end up tangent

1) You didn't say that in the original post

2) This is a MUCH more difficult problem (maintaining both tangency and tolerance)

 

In lieu of other solutions, one possibiity is:

- create lines/arcs using "simplify curve"

- then add fillets of an appropriate radius at each "non-tangent" curve transition

 

Calculating the fillet radius could be "interesting" (i.e. so tolerance is maintained)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Converting a spline to lines and arcs

Siemens Phenom Siemens Phenom
Siemens Phenom
The lines and arcs produced by the Simplify function **are** tangent (or, at least, they are supposed to be)
山田
yamada