Cancel
Showing results for 
Search instead for 
Did you mean: 

Create G1 Constraint

Builder
Builder

Dear all,

 

I want to write a VB code to create a spline through points in Sketch environment. But I want to create G1 constraint between the start point of the spline with the end point of an existing spline. I tried to record a Journal but it didn't help me. I will thank you if anyone can help me.

 

I use NX 11

Sina Shojaee
1 REPLY 1

Re: Create G1 Constraint

Phenom
Phenom

Look at the documentation for SketchG1Constraint Class.

Suresh
Technisites Australia
Production: NX10.0.3 Developing: NX11.0.2.7, NX12.0.2, NX1847,
Development: C++, C# .Net, VB .Net, Python, KF