Cancel
Showing results for 
Search instead for 
Did you mean: 

Create a new load case (results) to use AskNMinMaxLocation()?

Gears Phenom Gears Phenom
Gears Phenom

To all

 

Thinking loud here so don't throw stones. I investigated the use of function AskNMinMaxLocation(), see original query link at end of the question, to extract the "Top 10" stress (for a given list of elements for a given load case and iteration in the accessed results).

 

It seems than the function will return the top N for all the elements in the results. No what I have in mind.

 

So what if one was to;

  1. create a new (dummy) load case (result) based on load case and iteration selected for the elements selected
  2. create a new result based on #1 (load case 99999999 and iteratin 0)
  3. use AskNMinMaxLocation(), on result created in #2
  4. delete dummy load created in #1

I have not found anything on how to create a new load case based on an existing results for a given list of elements but maybe something like CAE.ResultsEnvelopeBuilder might be usefule

 

Any thought on the validity  and/or practicality of such approach?

 

Thanks

Regards

 

1st query: http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/use-of-function-AskNMinM...

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)