Cancel
Showing results for 
Search instead for 
Did you mean: 

Create an Password Protected VB Code

Pioneer
Pioneer

Hi

I have written some VB code and constantly using it my Computer .

I have some many macros and VB code created as shortcut in my NX Window.

I would like to share it with other people but i dont want the code to be shared .

How would give them like a role and or an icon so that anybody can run that macro/vb without able to read/write the code.

 

Suggest Please

 

4 REPLIES

Re: Create an Password Protected VB Code

Experimenter
Experimenter

Hi

Why dont you convert your VB into .dll or .exe using Visual Studio, where you dont need to worry about changes made to code by any one. Since .dll or .exe cannot be edited.

 

Regards

 

Re: Create an Password Protected VB Code

Pioneer
Pioneer

Thanks for reply.

I wonder if i could have 10 journels in my PC and i assign  10 command buttons to it (for easy understanding as an icon in the tool bar) and each have a path file to it.

 

Now i would like to give those 10 command buttons to the nearest colleague as role.Now say i have converted them as .dll or .exe file (unreadeable/uneditable by him).But i have assign all 10 command button paths to him which makes life complicated when more numbers are there.

 

I would like to export them as role /whatever possible method and assign the same on his PC but without assigning the path for all.

 

Is there any possible way of doing it?

 

As when you open NX i would like to find all the shortcut i have created (10 command buttons) and they should be propobly working on any number of system without any clue for anyone how does it work.(Same as NX buttons)

 

Suggestions are welcomed the most.

 

Re: Create an Password Protected VB Code

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Re: Create an Password Protected VB Code

Siemens Phenom Siemens Phenom
Siemens Phenom

See "Customizing the NX Interface using files" in the online help:

 

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api#uid:index_menuscript:xid923238