Cancel
Showing results for 
Search instead for 
Did you mean: 

Create an isometric view of a feature, VB.NET

Valued Contributor
Valued Contributor

I tried to record the journal but it is lengthy and returns too many errors when I edited some things.  

What I would like to do is to create an isometric view of body(1) of an assembly which is visible on layer 101 at ratio of 2:1. This requires making all layers invisible except the 101.

 

Any help is appreciated. 

 

 

1 REPLY

Re: Create an isometric view of a feature, VB.NET

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @ulink2rle,

 

Record the journal using the simple steps/process so that it should run/work on other parts also without any problem. ( I am not the journal expert, learning it Smiley Tongue)

 

I have recorded the journal (in NX 10) and run it on another part. There is no problem for me. Attached the video of the same along with journal file. I have used an isometric view with 2:1 scale and used layer 101 for the body as per your requirement. Tried journal in NX 9, works fine.