cancel
Showing results for 
Search instead for 
Did you mean: 

Create custom command in .tbr .men .rtb etc file for favorite .fav command

Pioneer
Pioneer

You can create a custom command in .tbr .men .rtb etc from a journal .vb file file as per below:

 

BUTTON MY_CMD_1

LABEL My Command

BITMAP ${MY_ENV_VAR}\MY_CMD.bmp

ACTION ${MY_ENV_VAR}\MY_CMD.vb

 

Can you do the same with favorites (.fav files)?

 

Regards,

Clayton McPherson
TC 10.1, NX 9.0.3.4 MP7
2 REPLIES

Re: Create custom command in .tbr .men .rtb etc file for favorite .fav command

Pioneer
Pioneer

Found example in the OOTB .men file

 

  BUTTON UG_INFO_SIMPLE_GEOMETRIC_DISTANCE PRIMARY=UG_INFO_GEOMETRIC_DISTANCE,FAVORITE="SimpleDistance"
  LABEL &Simple Distance...
  TOOLBAR_LABEL Simple Distance
  MESSAGE Calculates the distance between two objects.
  SYNONYMS measurement
  HELP UGS:: DlogUI::UICompMeasureDistance
  BITMAP distance
  ACTIONS STANDARD

Regards,

Clayton McPherson
TC 10.1, NX 9.0.3.4 MP7

Re: Create custom command in .tbr .men .rtb etc file for favorite .fav command

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Clayton,

No, favorites are specific to the existing NX dialog and essentially capture a particular state of that existing dialog. The favorite is like dialog memory for just the given dialog.

 

HTH, Joe