cancel
Showing results for 
Search instead for 
Did you mean: 

Curve collector's "Connected Curve" without the selection

Valued Contributor
Valued Contributor

Hello,

 

I currently have an unordered list of curves. I need to identify a subset of the list of curves that are touching,  end to end, within a tolerance. The functionality that I'm seeking already exists in the "Connected Curve" option of the Curve Collector's curve selection intent. In my case however, all the curves have already been acquired, so a selection is not desired. 

 

I'm wondering if the code that NX uses to determine how to select a chain of connected curves is available to us. I have been thus far unsucessful with any journal recording attempts, and my search through the API has been not helpful. 

 

Thanks,

jgolen

 


NX 9.0.3.4
MP13

NX 9.0.3.4 MP13
VB.net
Visual Studio 2015
5 REPLIES

Re: Curve collector's "Connected Curve" without the selection

Siemens Phenom Siemens Phenom
Siemens Phenom

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&dt=nx-api&q=sample+prog...

 

If that link fails, please search the solution center for "nx_api639", and it should find the example.

 

This example works with an array of selected curves, but if you already have them you can just pass them into the sort_end_to_end() function.

Re: Curve collector's "Connected Curve" without the selection

Valued Contributor
Valued Contributor
Nice, this is exactly what I was looking for, however, I forgot to mention that I write in VB.net. Do you have any solutions in VB.net? Otherwise I will convert this.

Thanks
NX 9.0.3.4 MP13
VB.net
Visual Studio 2015

Re: Curve collector's "Connected Curve" without the selection

Siemens Phenom Siemens Phenom
Siemens Phenom

No, sorry, we don't have that one in VB.  But I think the UF calls are all available as wrappers, so hopefully it won't be too much trouble to translate the sorting logic.

 

Re: Curve collector's "Connected Curve" without the selection

Valued Contributor
Valued Contributor
No problem, I'm already in the process of converting it and it doesn't seem to be too much trouble. Thanks again for the file!
NX 9.0.3.4 MP13
VB.net
Visual Studio 2015

Re: Curve collector's "Connected Curve" without the selection

Experimenter
Experimenter

Hi,

 

Could you share your code showing "connected curves" selection in VB.net?

 

Thanks

Marcin