Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom toolbar greyed-out until a file is opened - How to?

Phenom
Phenom

To all,

 

Is there a way of having the customised menu greyed-out until a .sim, .a fem , etc is opened? I saw the HIDE option but it's not what I want

 

Thanks

Regards

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)
4 REPLIES

Re: Custom toolbar greyed-out until a file is opened - How to?

Esteemed Contributor
Esteemed Contributor

You can make the .MEN file application specific.

Depending on the NX release there are different ways of doing so.

 

What NX release are you using?

Have you checked the menuscript reference on adding application specific menu files?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Custom toolbar greyed-out until a file is opened - How to?

Phenom
Phenom

NX9 & 10

Just re-read the doc and still a bit confused (but then the whole NX documentation is confusing!). I think I found what I had in mind but it's not a simple answer. Cannot be that difficult to write a couple of pages describing the steps to follow with a good/typical example! Anyway. I have my .men and an .rtb file in my /startup directory and I cannot figure out which one is picked up by NX when lauching the app.

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Custom toolbar greyed-out until a file is opened - How to?

Genius
Genius
for application specific Ribbons you need to go to your UGII_SITE_DIR folder (for example) and create an "application" folder.
Then create a "profiles" folder under "application" and then e.g. a folder named "UG_APP_MODELING" under "profiles".
If you put a *.RTB file there it will be specific to modeling application.
You can find the folder names under "%UGII_BASE_DIR%\UGII\menus\profiles\"

Re: Custom toolbar greyed-out until a file is opened - How to?

Esteemed Contributor
Esteemed Contributor

There is a best practice guide available for the ribbon bar, which is very good.

Search this forum for "ribbon" and you should get some useful hits.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community